This section contains various data sets where a manufacturer can add additional information about their products. These data sets can include performance data, additional classifications, sustainability information etc.
Each property set will contain parameters that you can fill in. You do not need to complete the entire set, just fill in the parameters that apply to your product. To expand the property set just select the arrow on the right side of the screen.

Fields within the property sets can have more than 1 value. To add multiple values, simply separate each value with a “ | “ (Vertical line).
Units can be selected through the drop down on the right hand side of the input field. Selecting “Range” will split the input field into two separate fields representing a minimum and maximum value.
At the bottom right corner of the expanded property set you'll be able to preview how your properties will look on the product and/or save your entries before moving to the next property set.
Available Property Sets
AEC Daily - AEC Daily is an E-Learning platform and host AECO certification courses as well continuing education programs in North America. You can add a link to an AEC Daily course or certification program for the intended product
Amazon - Information pertaining to the product if listed on Amazon including a direct link to “Buy” the product.
Architonic - a product hosting platform. You can add additional links and information of the same product if it’s listed on Architonic.
BIMobject SEEK Properties - a BIMobject property set that allows the inclusion of product specific information like materials, performance characteristics, etc.
BSD SpekLink - link to master format specification as well as link to Product Master Spec specifications
COBie UK - Construction Operations Building Information Exchange (COBie) is a non-proprietary data format for the publication of a subset of building information models (BIM) focused on delivering asset data as distinct from geometric information. This set is important to UK based end users.
Mortarr - Website that showcases construction projects and ideas. You can include a link to a project listed on Mortarr if you product is being used or showcased in that project.
RSK Databasen - Swedish data base that contains product information for plumbing and HVAC products. Just add the RSK product number in the field.
Sustainability - Various EPD (Environmental Product Declaration) Data sets. An Environmental Product Declaration (EPD) is a comprehensive, internationally-harmonized report that documents the ways in which a product, throughout its lifecycle, affects the environment.
Video here